Raw Main Time (Custom OFDM)
trace is the raw time data acquired directly from either the input hardware or playback file. Raw Main Time is used to generate the Search Time data which is the resampled and corrected Raw Main Time data. The Search Length parameter is used to specify the amount of Raw Main Time data.
The Meas Setup " Time parameter is not available (disabled) when the VSA is in modulation analysis mode.
See Also