EVM (Digital Demod)
(Error Vector Magnitude) is the Root Mean Square (RMS) of the error vectors computed and expressed as a percentage of theThe error vector magnitude is the length of the vector—at the detected symbol location—which connects the I/Q reference-signal vector to the I/Q measured-signal vector. The following graphic shows the calculation of the
metric as well as a diagram showing how a single error vector is calculated.
For constellations with constant magnitude (QPSK Quadrature phase shift keying, BPSK Binary phase shift keying - A type of phase modulation using 2 distinct carrier phases to signal ones and zeros., 8PSK, etc.), the EVMs are always normalized to the constellation maximum. For constellations with multiple possible magnitudes (APSK, StarQAM, 16QAM, 32QAM, etc.), the EVMs are normalized to the EVM Normalization Reference.
Shaped OQPSK Offset Quadrature Phase Shift Keying: A type of QPSK modulation that offsets the bit streams on the I and Q channels by a half bit. This reduces amplitude fluctuations and helps improve spectral efficiency. and Offset QPSK use two points-per-symbol (symbols and midpoints between symbols) to compute EVM and peak EVM due to the offset between I and Q.
For Offset QPSK, when the Half Sine Filter is selected, the OQPSK reference constellation points fall on a circle with a magnitude of sqrt(2)/2, but the EVM is still expressed as a percentage of the magnitude of a QPSK symbol point (magnitude = 1).
For the EDGE Enhanced Data for Global Evolution: A technology that gives GSMA and TDMA similar capacity to handle services for the third generation of mobile telephony. EDGE was developed to enable the transmission of large amounts of data at a high speed, 384 kilobits per second. (It increases available time slots and data rates over existing wireless networks.) demodulation format, the EVM, Phase, and Magnitude Error data results may vary for different settings. When is set to 1 (default), the trace data results are compensated for ISI Inter-Symbol Interference: An interference effect where energy from prior symbols in a bit stream is present in later symbols. ISI is normally caused by filtering of the data streams. (inter-symbol interference). For greater than one, the trace data results are not compensated for the effects of ISI.
If the EVM is larger than expected, see the troubleshooting tips in Troubleshooting.
See Also