Using Standard Setups/Presets (Digital Demod)

The following table lists the standard presets supported by the VSA. Click on a link to view the default parameter settings for that standard:

Available "Preset to Standard" Formats

Cellular

Wireless Networking

Digital Video

Other

CDMA BASE

Bluetooth®

J.83A/DVB-C (EUR)

APCO-25

CDMA MOBILE

HIPERLAN/1 (HBR)

J.83B/DOCSIS (NA) APCO- 25 P2 (HCPM)

CDPD

HIPERLAN/1 (LBR)

J.83C/ISDB-C (JPN) APC-25 P2 (HDQPSK)

EDGE

WLAN (802.11b)

DVB-S2 16APSK DECT

GSM

Wi-SUN

DVB-S2 32APSK TETRA

NADC

ZigBee 868 MHz

ATSC VDL Mode 3 

PDC

ZigBee 915 MHz

ATSC-M/H MIL-STD 188-181C:CPM(Opt 21)

PHP (PHS)

ZigBee 2450 MHz

  SOQPSK-TG (IRIG 106-04)

W-CDMA

 

  SOQPSK-A
      SOQPSK-B

In the following tables, to convert symbols to seconds, divide by the symbol rate.

  Preset-To-Standard Format

     Parameter

NADC North American Digital Cellular

PDC Personal or Pacific Digital Cellular: A Japanese standard for digital mobile telephony in the 800 MHz and 1500 MHz bands. To avoid the previous problem of lack of compatibility between the differing types of earlier analog mobile phones in Japan (i.e. NTT type and US developed TACS type), digital mobile phones have been standardized under PDC. In the case of the PDC standard, primarily six channel TDMA (Time Division Multiple Access) technology is applied. PDC, however, is a standard unique to Japan which renders such phone units incompatible with devices which adopt the more worldwide prevalent GSM standard. Nevertheless, digitalization under the standard enables ever smaller and lighter mobile phones which in turn has spurred market expansion. As a result, over 93% of all mobile phones in Japan are now digital.

PHP Personal Handy Phone: The mobile hand-set used with the Japanese Personal Handy Phone system. (PHS 1) Personal Handy Phone System, or 2) payload header suppression: The process of suppressing the repetitive portion of payload headers at the sender and restoring the headers at the receiver.)

Demod Format

pi/4 DQPSK Differential Quadrature Phase Shift Keying: QPSK modulation using differential encoding of the digital information stream.

pi/4 DQPSK

pi/4 DQPSK

Frequency Span

75 kHz kiloHertz: A radio frequency measurement (one kilohertz = one thousand cycles per second).

75 kHz

625 kHz

Symbol Rate

24.3 kHz  

21 kHz

192 kHz

Filtering

 

 

 

- Measured  

root cosine

root cosine

root cosine

- Reference  

cosine

cosine

cosine

Alpha / BT Bandwidth Time Product

0.35

0.5

0.5

Points / Symbol

5

5

5

Result Length

157 symbols

135 symbols

111 symbols

Search Length

1175 symbols

1000 symbols

1100 symbols

Pulse Search

Selected

Selected

Selected

Constellation Sync Search

Cleared

Cleared

Cleared

Normalize IQ Traces

Selected

Selected

Selected

Clock Adjust

0.0

0.0

0.0

Back to Preset to Standard Table.

  Preset-To-Standard Format

Parameter

GSM Global System for Mobile Communications: Originally developed as a pan-European standard for digital mobile telephony, GSM has become the world’s most widely used mobile system. It is used on the 900 MHz and 1800 MHz frequencies in Europe, Asia and Australia, and the 1900 MHz frequency in North America and Latin America.

CDPD

DECT Digital European Cordless Telecommunications

Demod Format

MSK Minimum Shift Keying Type 1

MSK Type 2

FSK Frequency Shift Keying: A form of modulation using multiple carrier frequencies to carry the digital information. The most common is the two frequency FSK system using the two frequencies to carry the binary ones and zeros. 2  

Frequency Span

1.0 MHz Megahertz: A unit of frequency equal to one million hertz or cycles per second.

75 kHz

5 MHz  

Symbol Rate

270.83 kHz

19.2 kHz

1.152 MHz  

Filtering

 

 

 

- Measured  

Cleared

Cleared

Cleared

- Reference  

Gaussian

Gaussian

Gaussian  

Alpha / BT

0.3

0.5

0.5  

Points / Symbol

5

5

4  

Result Length

148 symbols

378 symbols

480 symbols

Search Length

1434 symbols

400 symbols

11,200 symbols

Pulse Search

Selected

Cleared

Selected

Constellation Sync Search

Cleared

Cleared

Cleared

Normalize IQ Traces

Selected

Selected

Selected

Clock Adjust

0.0

0.0

0.0  

Back to Preset to Standard Table.

  Preset-To-Standard Format

Parameter

CDMA Code Division Multiple Access: One of several digital wireless transmission methods in which signals are encoded using a specific pseudo-random sequence, or code, to define a communication channel. A receiver, knowing the code, can use it to decode the received signal in the presence of other signals in the channel. This is one of several "spread spectrum" techniques, which allows multiple users to share the same radio frequency spectrum by assigning each active user an unique code. CDMA offers improved spectral efficiency over analog transmission in that it allows for greater frequency reuse. Other characteristics of CDMA systems reduce dropped calls, increase battery life and offer more secure transmission. See also IS-95. BASE

CDMA MOBILE

W-CDMA

Demod Format

QPSK Quadrature phase shift keying  

OQPSK Offset Quadrature Phase Shift Keying: A type of QPSK modulation that offsets the bit streams on the I and Q channels by a half bit. This reduces amplitude fluctuations and helps improve spectral efficiency.  

QPSK

Frequency Span

2.6 MHz  

2.6 MHz  

5 MHz

Symbol Rate

1.2288 MHz

1.2288 MHz

3.84 MHz

Filtering

 

 

 

- Measured  

IS-95 base

Cleared

Root Cosine

 

base EQ

 

 

- Reference  

IS-95

IS-95  

Cosine

 

baseband

baseband  

 

Alpha / BT

---

---

0.22

Points / Symbol

4

4

5

Result Length

200 symbols

200 symbols

200 symbols

Search Length

---

---

2560 Syms

Pulse Search

Cleared

Cleared

Cleared

Constellation Sync Search

Cleared

Cleared

Cleared

Normalize IQ Traces

Selected

Selected

Selected

Clock Adjust

0.0

0.0

0.0

Bit Definitions

defined by IS-95

defined by IS-95

---

Back to Preset to Standard Table.

  Other Preset-To-Standard Formats

Parameter

APCO 25

APCO 25 P2 (HCPM)

APCO 25 P2 (HDQPSK)

Demod Format

4 FSK

CPM Continuous Phase Modulation (FM Frequency Modulation) 4 FSK

Frequency Span

40 kHz

25 kHz 25 kHz

Symbol Rate

4.8 kHz  

6 kHz 6 kHz

Filtering

 

   

- Measured  

rect

None rect

- Reference  

raised cosine

4RC rect

Alpha / BT

0.2

0.75 1

Points / Symbol

5

5 5

Result Length

200 symbols

168 symbols 180 symbols

Search Length

400 symbols

380 symbols 380 symbols

Pulse Search

Cleared

Selected Cleared

Constellation Sync Search

Cleared

Cleared Cleared

Normalize IQ Traces

Selected

Selected Selected

Clock Adjust

0.0

0.0 0.0
CPM Auto {h1,h2} ---

Cleared,

{1/3}[APCO-25 P2]

---

Back to Preset to Standard Table.

  Digital Video J.83A/DVB-C (EUR)    

Parameter

DVB 16

DVB 32

DVB 64

DVB 128

DVB 256

EU-DOCSIS 64QAM

EU-DOCSIS 256QAM

Demod Format

16 DVB QAM Quadrature Amplitude Modulation

32 DVB QAM

64 DVB QAM

128DVB QAM

256 DVB QAM

QAM 64 QAM 256

Frequency Span

8 MHz

8 MHz

8 MHz

8 MHz

8 MHz

8 MHz 8 MHz

Symbol Rate

6.9 MHz

6.9 MHz

6.9 MHz

6.9 MHz

6.9 MHz

6.952 MHz 6.952 MHz

Filtering

 

 

 

 

 

   

- Measured  

root raised cosine root raised cosine root raised cosine root raised cosine

root raised cosine

root raised cosine root raised cosine

- Reference  

raised cosine

raised cosine

raised cosine

raised cosine

raised cosine

raised cosine raised cosine

Alpha / BT

0.15

0.15

0.15

0.15

0.15

0.15 0.15

Points / Symbol

2

2

2

2

2

2 2

Result Length

800

800

800

800

800

800 800

Search Length

---

---

 ---

---

---

--- ---

Pulse Search

Cleared

Cleared

Cleared

Cleared

Cleared

Cleared

Cleared

Constellation Sync Search

Cleared

Cleared

Cleared

Cleared

Cleared

Cleared

Cleared

Normalize IQ Traces

Selected

Selected

Cleared

Cleared

Selected

Selected

Selected

Clock Adjust

0.0

0.0

0.0

0.0

0.0

0.0

0.0

Back to Preset to Standard Table.

  Digital Video DVB-S2 Preset-To-Standard Formats

Parameter

16APSK

32APSK

Demod Format

16 APSK

32 APSK

Frequency Span

50 MHz

50 MHz

Symbol Rate

25 MHz

25 MHz

Filtering

 

 

- Measured  

root raised cosine

root raised cosine

- Reference  

raised cosine

raised cosine

Alpha / BT

.35

.35

Points / Symbol

5

5

Result Length

180 symbols

180 symbols

Search Length

1175 symbols

1175 symbols

Pulse Search

Cleared

Cleared

Constellation Sync Search

Cleared

Cleared

Normalize IQ Traces

Selected

Selected

Clock Adjust

0.0

0.0

Ring Ratio

See chart below

See chart below

Back to Preset to Standard Table.

DVB APSK Ring Ratios  
 

16 APSK

32 APSK

Code Rate

R2 / R1

R2 / R1

R3 / R1

Code Rate 2/3

3.15

--

--

Code Rate 3/4

2.85

2.84

5.27

Code Rate 4/5

2.75

2.72

4.87

Code Rate 5/6

2.7

2.64

4.64

Code Rate 8/9

2.6

2.54

4.33

Code Rate 9/10

2.57

2.53

4.30

Back to Preset to Standard Table.

  Digital Video J.83B/DOCSIS (NA)

Parameter

64QAM

256QAM

Demod Format

64QAM 256QAM

Frequency Span

8 MHz 8 MHz

Symbol Rate

5.056941 MHz 5.360537 MHz

Filtering

   

- Measured  

root raised cosine root raised cosine

- Reference  

raised cosine raised cosine

Alpha / BT

0.18 0.12

Points / Symbol

2 2

Result Length

800 symbols 800 symbols

Search Length

--- ---

Pulse Search

Cleared Cleared

Constellation Sync Search

Cleared Cleared

Normalize IQ Traces

Selected Selected

Clock Adjust

0.0 0.0

Back to Preset to Standard Table.

  Digital Video J.83C/ISDB-C (JPN)

Parameter

64QAM

Demod Format

DVB QAM 64

Frequency Span

8 MHz

Symbol Rate

5.274 MHz

Filtering

 

- Measured  

root raised cosine

- Reference  

raised cosine

Alpha / BT

0.13

Points / Symbol

2

Result Length

800 symbols

Search Length

---

Pulse Search

Cleared

Constellation Sync Search

Cleared

Normalize IQ Traces

Selected

Clock Adjust

0.0

Back to Preset to Standard Table.

  Digital Video ATSC and ATSC-M/H Preset-To-Standard Formats

Parameter

DTV 8

DTV 16

Demod Format

VSB 8

VSB 16

Frequency Span

7 MHz

7 MHz

Symbol Rate

10.762 MHz

10.762 MHz

Filtering

 

 

- Measured  

root cosine

root cosine

- Reference  

cosine

cosine

Alpha / BT

0.1152

0.1152

Points / Symbol

2

2

Result Length

800

800

Search Length

---

---

Pulse Search

Cleared

Cleared

Constellation Sync Search

Cleared

Cleared

Normalize IQ Traces

Selected

Selected

Clock Adjust

0.0

0.0

Back to Preset to Standard Table.

  Preset-To-Standard Format

Parameter

EDGE Enhanced Data for Global Evolution: A technology that gives GSMA and TDMA similar capacity to handle services for the third generation of mobile telephony. EDGE was developed to enable the transmission of large amounts of data at a high speed, 384 kilobits per second. (It increases available time slots and data rates over existing wireless networks.)

Bluetooth

WLAN WLAN - Wireless Local Area Network: A system that includes the distribution system (DS), access points (APs), and portal entities. It is also the logical location of distribution and integration service functions of an extended service set (ESS). A WLAN system contains one or more APs and zero or more portals in addition to the DS. (802.11b)

Demod Format

EDGE (3p/8 8PSK)

FSK 2

QPSK

Frequency Span

625 kHz

2.5 MHz

36 MHz‡

Symbol Rate

270.83 kHz

1 MHz

11 MHz

Filtering

 

 

 

- Measured  

EDGE(Windowed RC Radio Configuration: defines the physical channel configuration of cdma2000 (IS-2000) signals. Each RC specifies a set of data rates based on either 9.6 or 14.4 kbps. RC1 is the backwards-compatible mode of cdmaOne for 9.6 kbps voice traffic. It includes 9.6, 4.8, 2.4, 1.2 kbps data rates and operates at Spread Rate 1 (SR1). RC3 is a cdma2000 specific configuration based on 9.6 kbps that also supports 4.8, 2.7, and 1.5 kbps for voice, while supporting data at 19.2, 38.4, 76.8, and 153.6 kbps. RC3 also operates at SR1. For more information see Keysight application note "Performing cdma2000 Measurements Today".)

Cleared

Cleared

- Reference  

EDGE

Gaussian

Gaussian

Alpha / BT

0.25

0.5

0.5

Points / Symbol

1

2

4

Result Length

142 symbols

320 symbols

1000 Syms

Search Length

1434 Syms 

1650 Syms

1434 Syms

Pulse Search

Selected

Cleared

Cleared

Constellation Sync Search

Cleared

Cleared

Cleared

Normalize IQ Traces

Selected

Selected

Selected

Clock Adjust

0.0

0.0

0.0

Equalization

Cleared

¾

¾

 

‡ If the acquisition hardware does not support the default frequency span, then the span will be set to the closest span that the acquisition hardware can support.

 

Back to Preset to Standard Table.

  Preset-To-Standard Format
 

Parameter  

HIPERLAN/1 (LBR)

HIPERLAN/1 (HBR)

TETRA Trans-European Trunked Radio. A communications system standard.

Demod Format

FSK 2

MSK Type 1

pi/4 DQPSK

Frequency Span

18.7 MHz

36 MHz

40 kHz

Symbol Rate

1.4705875 MHz

23.5294 MHz

18 kHz

Filtering

 

 

 

- Measured  

Cleared

Cleared

root cosine

- Reference  

Rect  

Gaussian

cosine

Alpha / BT

--

0.3

0.35

Points / Symbol

20

5

4

Result Length

1000 symbols

1000 symbols

231 symbols

Search Length

1434 Syms

1434 Syms

1300 symbols

Pulse Search

Cleared

Cleared

Selected

Constellation Sync Search

Cleared

Cleared

Cleared

Normalize IQ Traces

Selected

Selected

Selected

Clock Adjust

0.0

0.0

0.0

Equalization

--

--

-

Back to Preset to Standard Table.

  Preset-To-Standard Format

Parameter

VDL Mode 3

Demod Format

D8PSK

Frequency Span

25 kHz

Symbol Rate

10.5 kHz

Filtering

 

- Measured  

Cleared

- Reference  

raised cosine

Alpha / BT

0.6

Points / Symbol

5

Result Length

315 symbols

Search Length

120 msec

Pulse Search

Selected

Constellation Sync Search

Cleared

Normalize IQ Traces

Selected

Clock Adjust

0.0

Back to Preset to Standard Table.

  Wi-SUN Preset-To-Standard Format    

Parameter

2-FSK 50/1

2-FSK 100/1

2-FSK 100/0.5

2-FSK 150/0.5

2-FSK 200/1

2-FSK 200/0.5

2-FSK 300/0.5

Demod Format

2-FSK

2-FSK

2-FSK

2-FSK

2-FSK

2-FSK

2-FSK

Frequency Span

200 kHz

400 kHz

400 kHz

600 kHz

800 kHz

800 kHz 1.2 MHz

Symbol Rate

50 kHz

100 kHz

100 kHz

150 kHz

200 kHz

200 kHz 300 kHz

FSK Deviation Reference (Manual)

25 kHz

50 kHz

25 kHz

37.5 kHz

100 kHz

50 kHz 75 kHz

Filtering

 

 

 

 

 

   

- Measured  

None

None

None

None

None

None

None

- Reference  

Gaussian

Gaussian

Gaussian

Gaussian

Gaussian

Gaussian

Gaussian

Alpha / BT

0.5

0.5

0.5

0.5

0.5

0.5 0.5

Points / Symbol

20

20

20

20

20

20 20

Result Length

2560

2560

2560

2560

2560

2560 2560

Search Length

---

---

 ---

---

---

--- ---

Pulse Search

Cleared

Cleared

Cleared

Cleared

Cleared

Cleared

Cleared

Constellation Sync Search

Cleared

Cleared

Cleared

Cleared

Cleared

Cleared

Cleared

Normalize IQ Traces

Selected

Selected

Cleared

Cleared

Selected

Selected

Selected

Clock Adjust

0.0

0.0

0.0

0.0

0.0

0.0

0.0

Back to Preset to Standard Table.

  Preset-To-Standard Format

Parameter  

ZigBee 868 MHz

ZigBee 915 MHz

ZigBee 2450 MHz

Demod Format

BPSK Binary phase shift keying - A type of phase modulation using 2 distinct carrier phases to signal ones and zeros.

BPSK

O-QPSK

Frequency Span

1 MHz

2 MHz

10 MHz

Symbol Rate

300 kHz

600 kHz

1 MHz

Filtering

 

 

 

- Measured  

Cleared

Cleared

Cleared

- Reference  

raised cosine

raised cosine

Half Sine

Alpha / BT

1

1

---

Points / Symbol

4

4

10

Result Length

1000 symbols

1000 symbols

1001 symbols

Search Length

10 ms

5 ms

3 ms

Pulse Search

Selected

Selected

Selected

Constellation Sync Search

Cleared

Cleared

Cleared

Normalize IQ Traces

Selected

Selected

Selected

Clock Adjust

0.0

0.0

0.0

Back to Preset to Standard Table.

  Preset-To-Standard Format      

Parameter  

MIL-STD 1) abbrevation for "standard" or 2) Selective Transmit Diversity: A transmit diversity technique using multiple base stations to originate the signal and provide spatial diversity on the downlink. In STD, the transmitter selection is based on a QoS measurement made at the mobile station. See also transmit diversity, TDTD and TSTD. 188-181C:CPM(Opt 21)

SOQPSK-TG (IRIG 106-04)

SOQPSK-A

SOQPSK-B

Demod Format

CPM (FM) Shaped OQPSK Shaped OQPSK Shaped OQPSK

Frequency Span

25 kHz 12.8 MHz 12.8 MHz 12.8 MHz

Symbol Rate

4.8 kHz 5 MHz 5 MHz 5 MHz

Filtering

       

- Measured  

None None None None

- Reference  

1REC SOQPSK-TG (IRIG 106-04) SOQPSK-A SOQPSK-B

Alpha / BT

0.35 0.35 0.35 0.35

Points / Symbol

5 10 10 10

Result Length

500 symbols 1000 symbols 1000 symbols 1000 symbols

Search Length

800 symbols -- -- --

Pulse Search

Cleared Cleared Cleared Cleared

Constellation Sync Search

Cleared Cleared Cleared Cleared

Normalize IQ Traces

Selected Selected Selected Selected

Clock Adjust

0.0 -- -- --
CPM Auto {h1,h2}

Selected,

{5/16,6/16}

-- -- --
OQPSK Align I and Q -- Cleared Cleared Cleared

See Also

Format tab (Digital Demod Properties)

Selecting Digital Demodulation

Setting up a Digital Demod Measurement

Troubleshooting (Digital Demod)