Carr Ofst (Digital Demod)
(Carrier Offset) shows the carrier frequency error relative to the VSA's center frequency. This error data is displayed in Hertz and is the amount of frequency shift, from the VSA's center frequency, that the VSA must perform to achieve carrier lock.
Errors in RF Radio Frequency: A generic term for radio-based technologies, operating between the Low Frequency range (30k Hz) and the Extra High Frequency range (300 GHz). frequency or LO frequency can appear as carrier offset.
is computed using all points (including points between symbols).