Freq Err (Digital Demod)
(Frequency Error) shows the carrier's frequency error relative to the VSA's center frequency. This error data is displayed in Hertz and is the amount of frequency shift from the VSA's center frequency that the VSA must perform to achieve carrier lock.
Errors in RF Radio Frequency: A generic term for radio-based technologies, operating between the Low Frequency range (30k Hz) and the Extra High Frequency range (300 GHz). frequency, LO frequency, or digitizer clock rate can all appear as carrier frequency error.
is computed using all points (including points between symbols).
Maximum frequency offset for reliable carrier lock
The following table shows the maximum frequency offset for which the demodulator will still be able to achieve reliable carrier lock when Result Length = 1000 symbols.
|
Digital Modulation Format |
Maximum frequency offset (Result Length = 1000 symbols) |
|---|---|
| 9.6% symbol rate | |
| 4.8% symbol rate | |
|
32 QAM |
3.15% symbol rate |
|
64 QAM |
4.65% symbol rate |
|
128 QAM |
0.3% symbol rate |
|
256 QAM |
0.3% symbol rate |
|
512 QAM |
0.15% symbol rate |
|
1024 QAM |
0.15% symbol rate |
|
2048-QAM |
0.1% symbol rate* |
|
4096-QAM |
0.1% symbol rate* |
|
16 DVB QAM |
4.65% symbol rate |
|
32 DVB QAM |
2.85% symbol rate |
|
64 DVB QAM |
4.65% symbol rate |
|
128 DVB QAM |
0.45% symbol rate |
|
256 DVB QAM |
0.15% symbol rate |
*Using Low SNR Signal-to-Noise Ratio Enhancement is required to make frequency locking robust for this QAM format.