ZeroCrErr (Digital Demod)
(Zero Crossing Error) is the calculated variation of the zero crossing of the measured signal, relative to the reference signal. The IEEE Institute of Electrical and Electronics Engineers. A US-based membership organisation that includes engineers, scientists, and students in electronics and related fields. The IEEE developed the 802 series wired and wireless LAN standards. Visit the IEEE at http://www.ieee.org standard document defines the acceptable zero crossing tolerance (e.g., 802.15.4g-2102 section 18.1.2.3.2). If you are measuring for conformance, the zero crossing error should fall within the standard's specified zero crossing tolerance.
Zero crossing error is calculated as a percentage of the symbol time.
Points between symbols are not used to compute the deviation offset.
Zero crossing error is computed for the following Format:.