Adaptive (Digital Demod)
Set to to have the VSA update the with each measurement (default). Set to to stop updating the .
This parameter is available only when the Equalization Filter check box is selected.
The VSA combines the previous measurement with the previous equalization filter coefficients to compute new filter coefficients. For the first measurement after the is reset, the VSA defines the to have a unit impulse response.
See Also