SOQPSK-TG (IRIG 106-04) (Digital Demod)
The filter equations are defined in section 2.4.3.2 of the following document: http://www.irig106.org/docs/106-05/chapter2.pdf. The filter parameters for supported SOQPSK variants are listed below.
|
SOQPSK Type |
ρ |
B |
T1 |
T2 |
|
SOQPSK-TG (IRIG 106-04) |
0.70 |
1.25 |
1.5 |
0.50 |
|
SOQPSK-A |
1.0 |
1.35 |
1.4 |
0.6 |
|
SOQPSK-B |
0.5 |
1.45 |
2.8 |
1.2 |
See Also