Excluded SubCarriers From MER (DOCSIS 4.0 Downstream)
Displays the results of the Excluded Subcarriers from MER Calculation parameter. This value will be empty (***) if the parameter is set to Off. Otherwise, the auto detected subcarriers or user manually excluded subcarriers will be displayed, and VSA will not calculate MER results for those subcarriers. The subcarrier indexes range from 0 to FFT-1 (4095 or 8191).
A displayed value of "***", "-780dB" or "-999" means no data is available.
See Also
Available Error Summary Results