IQ Offset (DOCSIS 4.0 Downstream)
(also called I/Q origin offset) indicates the magnitude of the carrier feedthrough signal. When there is no carrier feedthrough, IQ offset is zero (-infinity dB).
IQ Offset is the same as IQ Offset for Digital Demodulation. For more information about this parameter, see IQ Offset (Digital Demod).
A displayed value of "***", "-780dB" or "-999" means no data is available.
See Also