MER Pk (DOCSIS 4.0 Downstream)
is the peak level of the Modulation Error Ratio (MER) in the Measurement Interval. The value is shown in dB, and the symbol and subcarrier location of the peak are shown as well.
"Peak" refers to the peak error (minimum MER).
See Also