MER (DOCSIS 4.0 Downstream)
is the average value of the Modulation Error Ratio (MER) over the entire measurement interval (includes PLC, Pilot, and Data subcarriers), expressed in decibels (dB).
A displayed value of "***", "-780dB" or "-999" means no data is available.
See Also