OFDM BER/MER Summary (DOCSIS 4.0 Downstream)
The trace shows the Bit Error Ratio (BER), Modulation Error Ratio (MER), and Codeword Error Ratio (CWER) for each profile used.
A displayed value of "***", "-780dB" or "-999" means no data is available.
Mod Format
- The modulation format is a detected QAM value. NCP can only be QPSK, 16 QAM, or 64 QAM.
MER
- The average value of the Modulation Error Ratio (MER).
- is the peak level of the Modulation Error Ratio (MER).
BER/CWER
BER/CWER measurements only show when BER Analysis is selected under the Format tab.
- You can accumulate bit counts by enabling measurement averaging (Analysis > Average > RMS or RMS Exponential). The Pause Measurement after Bit Count feature uses the Bits before LDPC count.
- Bit error count before LPDC. After LPDC, codeword errors are measured instead of bit errors.
- Ratio of bit errors to total bits before LPDC. After LPDC, codeword errors are measured instead of bit errors.
- Total number of codewords processed for CWER.
- Codeword Error count after multiple iterations of the LDPC decoder and before the BCH decoder.
- Codeword error ratio after multiple iterations of the LDPC decoder and before the BCH decoder.
- Codeword error count after the BCH decoder.
- Codeword error ratio after the BCH decoder.
- Average number of LDPC iterations used over all codewords in a profile.
- Maximum number of LDPC iterations used over all codewords in a profile. The maximum number of iterations used in decoding is 20.
About Profiles
There are up to 16 profiles (A-P) plus NCP. The corresponding profile IDs are 0-15 for A-P and 255 for NCP.
When Initial Settings = Auto, only NCP and Profile A can be demodulated. Other profiles will be detected and shown in the BER/MER summary, but detected profiles B-P will display "Unknown" in the Mod Fmt row and undesirable MER values. This is an indication that the signal has B-P profiles that need to be manually defined to get correct overall MER and BER measurements for the signal. Unless the profiles corresponding to these code words are defined, VSA can not determine the modulation type associated with the code word, and so it is not possible to accurately calculate the MER.
To manually define Profiles B-P, set Initial Settings to Manual and then edit the User Profiles vectors.
See Also