PDF (DOCSIS 4.0 Downstream)
trace data displays the Probability Density Function of the selected channel. PDF indicates the probability that a given level has occurred.
The PDF is computed from the segment of the OFDM burst specified by the Measurement Interval and Measurement Offset.
See the Reference PDF trace (Reference) topic for more detailed information about this trace data.
See Also
Available Trace Data (DOCSIS 4.0 Downstream)