Time Tab (DOCSIS 4.0 Upstream)
The Time tab of the DOCSIS 4.0 Upstream Demod Properties dialog box lets you access the signal capture configuration parameters. You use these parameters to select the search length for finding the frame boundary, and to isolate a segment of the time record for further viewing and data analysis.
The Time tab dialog box allows you configure these parameters:
- Search Length
- Result Length
- Measurement Offset
- Measurement Interval
- Enable Burst Search
- Burst Detection Threshold
See Also