Correction (DOCSIS 4.0 Upstream)
trace is the correction curve used to correct for the frequency response of the input hardware and input digital filtering. The correction trace is applied to the acquired data to compensate for phase and magnitude anomalies in the VSA's hardware and software signal processing.
See Also
Available Trace Data (DOCSIS 4.0 Upstream)