Eq Impulse Response (DVB-RCS2)
There are two types of traces in the Trace > Data > Demod menu that display component carrier data: CCn (component carrier is fixed), and Display CC (component carrier is dynamically selected using the Carrier Aggregation > Selected CC for Trace Display parameter). See About Demod Per-Carrier Trace Types for more information.
When is enabled and the equalizer is ON, the trace shows the impulse response of the equalization filter for the component carrier.
See Also