Meas Demod Bits (DVB-RCS2)

The Meas Demod Bits trace shows the bits after demodulation. The first bit in the table corresponds to the first bit of the first symbol.

By default, the bits are displayed in 8-bit bytes in hexadecimal format. Like other bit displays in the VSA software, Trace > Properties > Digital Demod > Symbol Table Format can be used to switch from hex to binary.

See Also

Available Trace Data