Meas Decoded Bits (DVB-RCS2)
The trace shows the decoded bits for the physical layer channels.
The level of encoding is determined by the BCH/LDPC Encode On parameter.
By default, the bits are displayed in 8-bit bytes in hexadecimal format. Like other bit displays in the VSA software, Trace > Properties > Digital Demod > Symbol Table Format can be used to switch from hex to binary.
See Also