Error Vector Spectrum (DVB-S2/S2X)
There are two types of traces in the Trace > Data > Demod menu that display component carrier data: CCn (component carrier is fixed), and Display CC (component carrier is dynamically selected using the Carrier Aggregation > Selected CC for Trace Display parameter). See About Demod Per-Carrier Trace Types for more information.
The trace shows the spectrum of the Error Vector Time trace. In other words, the VSA derives the trace and then windows and FFTs this trace to produce the trace.
The center frequency and span for the trace is identical to the IQ Meas Spectrum.