Inst IQ Ref Spectrum (DVB-S2/S2X)
There are two types of traces in the Trace > Data > Demod menu that display component carrier data: CCn (component carrier is fixed), and Display CC (component carrier is dynamically selected using the Carrier Aggregation > Selected CC for Trace Display parameter). See About Demod Per-Carrier Trace Types for more information.
When is enabled, is the instantaneous spectrum of the IQ Ref Time trace. In other words, is the non-averaged versions of IQ Ref Spectrum trace data.
See Also