Meas Demod Bits (DVB-S2/S2X)
The trace shows the bits after demodulation. The first bit in the table corresponds to the first bit of the first symbol.
By default, the bits are displayed in 8-bit bytes in hexadecimal format. Like other bit displays in the VSA software, Trace > Properties > Digital Demod > Symbol Table Format can be used to switch from hex to binary.
See Also