Troubleshooting (GSM/EDGE/EDGE Evolution)
This topic contains information to help you troubleshoot measurements when using the GSM Global System for Mobile Communications: Originally developed as a pan-European standard for digital mobile telephony, GSM has become the world’s most widely used mobile system. It is used on the 900 MHz and 1800 MHz frequencies in Europe, Asia and Australia, and the 1900 MHz frequency in North America and Latin America./EDGE Enhanced Data for Global Evolution: A technology that gives GSMA and TDMA similar capacity to handle services for the third generation of mobile telephony. EDGE was developed to enable the transmission of large amounts of data at a high speed, 384 kilobits per second. (It increases available time slots and data rates over existing wireless networks.)/EDGE Evolution demodulator. Also see Setting up a GSM/EDGE/Edge Evolution Measurement for additional measurement information.
|
PROBLEM |
POSSIBLE CAUSE |
SOLUTION |
|---|---|---|
|
Demodulation fails to lock on signal |
Signal not present |
Check connections |
|
|
Carrier too far from center frequency |
Adjust |
|
|
Input is over-loaded or under ranged |
Adjust |
|
|
Frequency span is too narrow |
Increase frequency |
|
|
Wrong symbol rate |
Enter correct |
|
|
Wrong modulation scheme |
Specify correct modulation scheme, or set Modulation Scheme to |
|
|
I/Q offset too large |
Reduce LO feedthrough (or DC offset for I+jQ receiver) |
|
Spectrum Disappears |
Spectrum not present or digital demodulation not configured correctly. |
View the spectrum trace (Trace > Data Spectrum) and also examine the time and search time traces (Trace > Data > Time or Trace > Data > Search Time). Use these traces to determine whether the spectrum is present and whether the digital demodulator is configured properly. |
|
|
|
|
| Eye diagrams show incorrect symbol timing |
I and Q are misaligned using I+jQ receiver |
Check cable lengths Adjust for delay using external calibration |
|
|
|
|
|
SYNC NOT FOUND |
Search length too short |
Increase |
|
|
Incorrect filter selection for HSR signal |
Make sure that the HSR Pulse Shape Filter parameter is set to for high symbol rate signals. |
|
|
|
|
|
PULSE NOT FOUND |
||
|
|
Search length too short |
Increase or adjust triggering to ensure that leading and trailing edges of pulse are fully within search length |
|
|
Signal length not optimized |
Try the following method to determine when performing a Pulse Search: SL = (2*MaxOn) + MaxOff Where:SL is search length in seconds. MaxOn is the maximum on time of a pulse in seconds. MaxOff is the maximum off time between pulses in seconds. |
|
|
|
|
|
Pulse found but incorrectly aligned |
Poor signal-to noise ratio or on/off ratio |
Check setting Reduce to eliminate excess noise and interfering signals. |
|
|
Time corrections disabled |
Enable time corrections |
|
|
Span is too narrow |
Increase span to prevent degradation of pulse edges |
|
|
|
|
|
Error Vector Time shows regions of large errors |
Distortion or a poor signal to-noise ratio causing bit errors |
Check |
|
|
Large frequency errors interfering with carrier lock |
Adjust |
|
|
Large I/Q offsets causing bit errors |
Reduce LO feedthrough (or DC offset if using I+jQ receiver) |
|
|
|
|
|
EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. larger than expected and Error Vector Time shows errors that increase towards beginning and end of result length |
Wrong symbol rate |
Make fine adjustments to the |
|
|
|
|
| EVM is high at the very start and very end of Error Vector Time, but good everywhere else | Signal has incorrect tail bits |
Set the Synchronization Mode to , or change the tail bits to match the GSM/EDGE/EDGE Evolution standards. Background: The tail bits are not shown but can affect EVM of neighboring bits when the is set to or . In these synchronization modes, the VSA uses a Viterbi decoder with built-in knowledge of both the TSC sequence and the tail bits in order to provide robust demodulation of noisy signals. The decoder will cause errors from the tail bits to "leak" into neighboring bits. |
|
EVM larger than expected and Error Vector Time shows a uniform distribution of errors |
Frequency span too narrow |
Increase |
|
|
Incorrect filter selection for HSR signal |
Make sure that the HSR Pulse Shape Filter parameter is set to for high symbol rate signals. |
|
|
Input is overloaded or under ranged |
Adjust |
|
|
Signal too close to DC |
Increase carrier |
|
|
I and Q misaligned using I+jQ receiver |
Check cable lengths Adjust for delay using external calibration |
|
|
AC coupling when using I+jQ receiver |
Select on both input channels |
|
|
I and Q imbalance |
Ensure impedance is identical for both inputs |
|
The trace data constellation symbol location shape, such as dots, is not properly displayed. |
The display driver is not functioning correctly. |
Contact your PC manufacturer to see if a newer version of the display driver is available. If not, try decreasing the hardware acceleration. See the Windows documentation for instructions. |
See Also
Setting up a GSM/EDGE/EDGE Evolution Measurement