AQPSK Subchannel Power Imbalance Ratio (GSM/EDGE/EDGE Evolution)
0 dB
-10 to 10 dB
specifies the power ratio, expressed in dB, of the two subchannels in the AQPSK constellation.
The Alpha value of the AQPSK constellation is defined as follows:
The angle of the ideal state positions of the AQPSK constellation is defined as follows:
See Also