Quick Setups... (Flex Frame)
displays a menu of predefined and custom Quick Setups. Selecting a Quick Setup from the menu will populate the Flex Frame Properties with the settings saved in the Quick Setup. Quick Setups do not change any settings outside of Flex Frame, except for .
Factory-supplied Quick Setups may be modified or deleted in future releases of the VSA software. For this reason, programmatic users should not use factory-supplied Quick Setups directly. Instead, load the factory-supplied Quick Setup and save it under a different name as a custom Quick Setup.
Quick Setups suffix types (in order, as displayed in menu*):
- Shared
- specifies a Quick Setup available to all users of the current workstation.
- Private
- specifies a Quick Setup available only to the current user.
- <no suffix>
- specifies a Quick Setup installed with the VSA.
* Each suffix group is sorted alphabetically.
A delete button
appears after each saved Quick Setup ( or ). Click this button if you no longer need a saved Quick Setup and want to remove it from the list. See Save As Quick Setup for more information on saved Quick Setups. Quick Setups that have no suffix are factory-supplied and cannot be deleted.
See Also