Exclude During Analysis

Analysis > FMCW Radar Properties > Time

You can specify a portion of each detected LFM region’s start and end time samples to be excluded from the FMCW region analysis results. This is useful when the detected LFM region contains known FM Frequency Modulation modulation transition and settling effects, which you want to exclude from the reported FMCW Region Table performance metrics.

The illustrations below show the same FMCW measurement with both start and end percent set to 0%, and again with both values set to 6%. Notice how the gap changes between regions 5 and 6.