Maximum Region Count

Analysis > FMCW Radar Properties > Time

When the Maximum Region Count check-box is enabled, you can specify an upper limit to the number of detected signal LFM regions which should be considered for inclusion within FMCW region analysis results.

If the measured signal contains more valid regions than Max Region Count, only the first Max Region Count number of detected signal regions will be processed and reported within FMCW region analysis results. When Max Region Count check-box is disabled, all valid detected signal LFM regions within the Acquisition Length time interval will be reported within FMCW region analysis results.

Default check-box state = On

Default value = 100 regions