Amplitude Meas Time
Menu Path:
Amplitude Meas Time reports region-synchronized measured signal amplitude level samples over time in the units determined by the Trace Y Scale and Trace Format selection combination.
When the Time Values Are Relative To is set to First Region, X-axis time values are displayed relative to the first detected region Time Start (s) value. When Time Values Are Relative To is set to Trigger, X-axis time values are displayed relative to the acquisition trigger event.
The Inst Amplitude Meas Time trace is a non-averaged version of Amplitude Meas Time .
The Y Scale units of the reported Amplitude trace can be configured from either the Trace menu or by right clicking the Amplitude Meas Time trace Y Scale trace area as follows:

By selecting the appropriate Y Unit and trace Format selection combination listed below, you can display Amplitude Meas Time trace results in either dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer, Watt, or Volt units:
- Y Unit = Auto: Format = Log Mag
- dBvPk units
- Y Unit = Auto: Format = Linear Mag
- Volt units
- Y Unit = Auto: Format = Real
- Volt units
Valid trace Format selections are:
- Log Mag (dB)
- Linear Mag
- Real