FM Slope Error Time
Menu Path:
FM Frequency Modulation Slope Error Time reports region-synchronized measured signal FM Slope error samples over time in Hz/us. ( FM Slope Error Time = FM Slope Meas Time - FM Slope Ref Time).
When Time Values Are Relative To is set to First Region, X-axis time values are displayed relative to first detected region Time Start (s) value. When Time Values Are Relative To is set to Trigger, X-axis time values are displayed relative to acquisition trigger event occurrence.
The Inst FM Slope Error Time is a non-averaged version of FM Slope Error Time.
Valid trace Format selections are:
- Real