FM Slope Meas Time
Menu Path:
FM Frequency Modulation Slope Meas Time reports region-synchronized measured signal FM Slope samples over time in Hz/us.
When Time Values Are Relative To is set to First Region, X-axis time values are displayed relative to first detected region Time Start (s) value. When Time Values Are Relative To is set to Trigger, X-axis time values are displayed relative to acquisition trigger event occurrence.
The Inst FM Slope Meas Time is a non-averaged version of FM Slope Meas Time.
Valid trace Format selections are:
- Real