Phase Error Time
Menu Path:
Phase Error Time reports region-synchronized measured signal phase error samples over time in degrees (i.e. Phase Error Time = Phase Meas Time - Phase Ref Time).
When Time Values Are Relative To is set to First Region, X-axis time values are displayed relative to the first detected region Time Start (s) value. When Time Values Are Relative To is set to Trigger, X-axis time values are displayed relative to the acquisition trigger event.
The Inst Phase Error Time is a non-averaged version of Phase Error Time.
Valid trace format selections are:
- Real