Y Bottom
The value of the lowest point on the Y-axis (magnitude). You can change Y Bottom by clicking the value one time to select it, then either double-click, start typing, or use the mouse wheel or the keyboard arrow keys to change the value. The grid always has 10 vertical divisions, so changing either Y Top or Y Bottom also changes the Y / Div value. |