Y Top
|
The value of the highest point on the Y-axis (magnitude). You can change Y Top by clicking the value one time to select it, then double-click to input a new value. Or you can just start typing or use the mouse wheel or the keyboard arrow keys to change the value. The grid always has 10 vertical divisions, so changing either Y top or Y bottom also changes the Y/Div value. |