Command Line Options
You can run the 89600 VSA Software from the Windows Start menu or from the command line.
To run the 89600 VSA software from the command line, open a Command window and run Agilent.SA.Vsa.Vector-x64.exe, which by default is located in the following location:
-
%ProgramFiles%\Keysight\89600 Software <ReleaseVersion>\89600 VSA Software\Agilent.SA.Vsa.Vector-x64.exe
The 89600 VSA software supports the following command line arguments:
|
/HELP:<value> |
shows the command line help. /HELP for all. /HELP:<name> for specific command details. Valid /HELP variations include /?, -?, /h, -h, /help and -help. |
|
|
/SETUP:<value> |
loads the named setup file at startup. |
|
|
/RECORDING:<value> |
loads the named recording at startup. |
|
|
/NOSEARCHHARDWARE |
skips the normal hardware discovery at startup. |
|
|
/ANALYZER:<value> |
uses the named analyzer hardware configuration. |
|
|
/SOURCE:<value> |
uses the named source hardware configuration. |
|
|
/NOSPLASH |
hides the splash screen at startup. |
|
|
/NOMESSAGE |
disables message dialogs. |
|
|
/PORT:<value> |
specifies the port number at which to listen for requests from .NET Framework clients. |
|
|
/SERVERADDRESS:<value> |
specifies where to listen for requests from .NET 6.0+ clients. <value> can be :host[:port]. |
|
|
/HISLIP:<value> |
specifies the HiSLIP device name to use for the SCPI server. |
|
|
/HWCONFIG:<value> |
specifies a hardware configuration to be created or modified for use at startup. Usage: /HWCONFIG:"<NameOfConfiguration>=[InstrumentType, ]Address1[;[InstrumentType, ]Address2|[InstrumentType, [Address3...]
The instruments specified will automatically be added to the VSA Instrument Manager and discovered at startup. |
|
|
/HOSTAPP:<value> |
specifies information for switching back and forth between VSA and a HostApp. |
You must include a switch character ("/" or "-") at the beginning of each option name.
If specifying more than one command line argument, separate each argument by a single space.
A command line argument ("xxx:yyy") must be enclosed within double quotes if there are any spaces in the "yyy" portion of the argument. Otherwise, quotes are not required.