Response Power (Graph)
is the RMS average power of the response signal, calculated over all points in the compensated stimulus time data (which can be viewed using the Response Time trace).
See Also
is the RMS average power of the response signal, calculated over all points in the compensated stimulus time data (which can be viewed using the Response Time trace).
See Also
|
Copyright © 2000-2026 Keysight Technologies, Inc. |