About this Reference
The Reference section of the documentation contains details about standard features available with Keysight 89600 VSA software. This section also describes the standard menu functions, associated parameters, and their operation.
Most feature descriptions apply to all measurement types, but some features apply only to the and measurement types (for example, Time Gating, Main Time Length, Frequency Points).
A separate section of documentation is provided for each digital modulation measurement type listed in the Optional Measurement Software book.
See Also