Connection (Input Analog Tab)
The parameter specifies the input impedance terminations on the measurement hardware for the selected Logical Channel.
The two options for are:
- Single-ended (unbalanced)
- Differential (balanced)
This parameter can be selected for channels or individually for each available channel. The available channels are displayed in located at the top of the dialog box. If the selections for individual channels are different, the arrow button (
) after the text box will be orange. Click the arrow button to view the selection for each available channel.
Some measurement hardware provides the following input impedance terminations:
|
Single-ended Termination: This refers to an unbalanced input termination. |
|
|
Differential Termination:This refers to a balanced input termination. |
|
For a list of supported hardware, see Measurement Hardware.
See Also