Holdoff Style (Trigger)
There are three trigger that determine how the trigger Holdoff is defined:
- - Trigger specifies the length of time following a trigger that must elapse before the next trigger can occur, regardless of the trigger Level set. This configures the measurement hardware to ignore trigger signals for a specified period of time
- - Trigger specifies an amount of time that the hardware's input signal must be a stable low value (below the trigger level) before the next trigger can occur.
- - Trigger specifies an amount of time that the hardware's input signal must be a stable high value (above the trigger level) before the next trigger can occur.
See Holdoff for more details.
Selections that are not available when using specific measurement hardware will be grayed out.
This trigger parameter is shared by measurements that share the same Analyzer Configuration. Changing this parameter for one shared measurement will change it for the other shared measurements.
Trigger parameters (including this one) affect the outcome of the time record capture from hardware when creating a recording as well as when making a measurement.
See Also