Trigger Tab (Input)
The tab sets up a trigger signal.
-
Input Trigger Channel: Selects which input channel to trigger on.
Only one channel can be used to trigger the measurement.
-
Style (Segmented Capture = Disabled): Determines the trigger type and trigger signal.
-
Gate Style (Segmented Capture = Enabled): Determines the trigger type and trigger signal.
-
Delay (Segmented Capture = Disabled): Determines the amount of time used for trigger delay. When Segmented Capture is enabled,
-
Gate Start Delay (Segmented Capture = Enabled): Determines the amount of time delay before each captured segment.
-
Gate Stop Delay (Segmented Capture = Enabled and Segment Type = Variable): Determines the amount of time delay after each captured segment.
-
Level: Sets the trigger level.
-
Slope: Sets the trigger slope.
-
Hold-off Style: Sets the trigger hold-off style.
-
Hold-off: Determines the amount of time used for trigger hold-off.
-
Periodic Trigger parameters: These parameters are used to set up and control the Periodic trigger style.
-
Period: Specifies the trigger interval.
-
Period Offset: Adds an offset relative to the periodic triggering point.
-
Sync Source: Determines how the first measurement is triggered.
-
-
Time Qualified Trigger (TQT) parameters: These are used to set an additional trigger criterion of time duration, which an event needs to last in order to satisfy the trigger (only shown when connected to an X-Series Analyzer with Real Time Spectrum Analyzer, and only available when Frequency Mask Trigger or IF Mag Style is selected).
-
Time Criteria: A menu of time-qualifying trigger choices using the Time1 and/or Time2 parameters.
-
Time1: Time duration 1, used by the Time Criteria setting for determining when and if to trigger.
-
Time2: Time duration 2, used by the Time Criteria setting for determining when and if to trigger.
-
-
Frequency Mask Trigger parameters: These parameters are used to set up and control the Frequency Mask trigger style--only shown when connected to an X-Series Analyzer with the Real Time Spectrum Analyzer (RTSA) option.
-
RBW:
-
-
Trigger Out: Selects the desired trigger output connector to use on the currently connected instrument.
-
Display Trigger Reference Line on Active Trace: Determines whether the trigger reference line is shown on the currently selected trace.
For multi-channel measurements, the same trigger style and parameters are applied to each channel. Any changes made for one channel are reflected in the setup for the other channel. Different trigger configurations cannot be specified for individual channels.
For information on triggering with specific measurement hardware, see Available Measurement Hardware for a link to your hardware.
See Also