Conversion Tab

When the Power Spectrum, Adjacent Channel Power or Spectral Emissions Mask measurement is selected, the Analysis dialog displays the Conversion tab, which enables you to control image protection parameters in your VSA hardware. The Conversion tab contains the following parameters:

See Also

Image Protection