ResBW Tab (MeasSetup)

The ResBW tab contains parameters related to the resolution bandwidth.

 

For Power Spectrum, Adjacent Channel Power and Spectral Emissions Mask measurements, the ResBW tab contains the following additional parameters for the resolution bandwidth and video bandwidth.

In case of zero span mode in Power Spectrum measurements, the Window Type parameter gets replaced with Channel Filter Shape parameter. Only the following values are available for this parameter:

See Also

About Windowing