Details (Frequency Reference)
Click the arrow to open the portion of the dialog box, listing the external reference state for each module. The state includes the presence or absence of an external reference signal and whether the module is locked to that signal.
A red X (
) next to the hardware indicates that the hardware
is not properly configured and locked. In this case, the measurement hardware
is not all referenced to the same frequency source. To change the configuration
or lock status, click the Configure
button in the corresponding tab in the dialog box.
See Also