System Reference Instrument (Frequency Reference)
The System Reference Instrument box lists the hardware the external reference signal is connected to. Select from the list to specify which hardware to use as the system reference.
See Also
The System Reference Instrument box lists the hardware the external reference signal is connected to. Select from the list to specify which hardware to use as the system reference.
See Also
|
Copyright © 2000-2025 Keysight Technologies, Inc. |