Marker Shortcuts
In addition to the menu, the following can be used to set up and move markers:
- mouse shortcuts
- keyboard shortcuts
- marker tools
Mouse shortcuts
-
Click on the marker tool icon of interest from the Markers Toolbar (Select Area tool
, Marker tool
, Band Power tool
, Time Gate tool
), then click and drag in the trace to place the marker. -
Right-click in the trace for a context menu with marker selections.
-
Drag the marker or just click the location for the currently selected marker to move.
-
Marker to peak: right-click in trace, click Peak.
-
When the Band Power tool is active and you hover the over one of the Band Power marker's edges, the cursor will change to a left-right arrow and you can drag the edge to change the band power span.
-
In the Markers Window, click anywhere on a marker readout line to select the corresponding marker as the active marker (the trace containing the marker will also be made the active trace). Double click the marker readout X position (or Z position) and type the marker position. The keyboard arrow keys or the mouse wheel can also be used to change the highlighted marker readout value, and move the marker.
- When there are multiple markers on a trace, click on the marker shape (diamond or 'X') to select the marker as the active marker.
-
For information on moving spectrogram markers with the mouse, see moving spectrogram markers.
Keyboard shortcuts
The following shortcuts all refer to marker search functions.
-
Home moves the marker to the first point
-
End moves the marker to the last point
-
Page Up moves the marker to peak
-
Page Down moves the marker to minimum
-
¬ moves the marker one point to the left
-
® moves the marker one point to the right
-
↑ moves the marker to the next larger peak
-
¯ moves the marker to the next smaller peak
-
Ctrl+ ¬ moves the marker to next peak to the left
-
Ctrl+ ® moves the marker to next peak to the right
Markers on OFDM traces
The information below describes only the differences in marker shortcut operation for OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. trace data that contains Z-axis information (OFDM Error Vector Spectrum and OFDM Error Vector Time, for example).
-
¬ moves the marker to the next smaller value along the x- or z-axis as specified by the active (highlighted) marker readout. To change axis, select the non-active x- or z-axis marker readout field.
-
® moves the marker to the next larger value along the x- or z-axis as specified by the active (highlighted) marker readout. To change axis, select the non-active x- or z-axis marker readout field.
-
↑ moves the marker to the next higher y-value along the z-axis for the current x-axis position. This key will not move the marker in the x-axis dimension.
-
¯ moves the marker to the next lower y-value along the z-axis for the current x-axis position. This operation will not move the marker in the x-axis dimension.
-
Ctrl+ ¬ moves the marker left one x axis point to the z axis point that has the nearest y value to the current marker y value.
-
+ ® moves the marker right one x axis point to the z axis point that has the nearest y value to the current marker y value.