Preset Setup

Clicking Preset > Setup removes all but the first measurement, sets the measurement type to Vector, and resets most of the parameters under the Input, Analysis, and Markers menus, and the trace layout.

In addition, Traces A and B are set to Ch1 Spectrum and Ch1 Main Time, respectively.

The following parameters are not modified: