Save Bitmap / Print dialog
From the and dialogs, a bitmap of traces and other tool windows can be saved or printed.
Save Bitmap dialog
In the dialog, you can choose what to save in an image file.
Content Selection
-
- selects which windows to save to a bitmap file. The entire window as shown on screen (including title bar and status bar) will be saved.
- - selects which trace windows and tool windows to save.
Only the first window/result selected will be saved unless the bitmap format chosen is TIFF. In this case, the selected windows/results will be saved as separate images in a single TIFF file.
Be aware that some image editing programs only know how to view the first image in a TIFF file.
Other controls
button: prompts the user for a file name and then exports the selected images to the file.
The bitmap may be corrupted on systems which meet one of these conditions:
- limited amount of graphics memory
- graphics memory has been consumed by a large number of open windows
- non-standard video encoders or drivers installed
The saved bitmap may be missing all or part of the desired screen area, or the bitmap may be scrambled. You may be able to work around this problem using alternate methods ("Print Screen" key, or the "Snipping Tool"). However, these may also fail depending on the original cause of the problem.
Print dialog
In the dialog, set up how the trace area is to print. All the settings, except , are remembered, even when the VSA application is stopped and restarted.
The dialog is composed of multiple collapsible sections. Click the name of a collapsible section to open and close the section.
Printer Selection
Using the dropdown box, select among the printers currently installed on your computer.
Content Selection
- : allows you to select which windows to print and prints the entire window except the title bar, menu bar, and status bar. The printed page will include visible traces and any docked tool windows, including the marker window.
- : prints only the selected traces and tool windows. Each view is printed on a separate page by default. To print more than one trace on a page, set the parameter to a value greater than 1.
Page Options
-
- : specifies a paper size to print on
- : specifies the printer tray to use
- : sets up margins from the four edges of the page
Layout Options
- : selects landscape or portrait page orientation. Some traces will fit better in one orientation than the other.
-
- : When is selected, the trace area is expanded until it reaches the maximum width or height of the page, whichever happens first. The image maintains the same aspect ratio as shown on the computer screen.
-
: When is selected, the trace area is expanded both horizontally and vertically to fill the whole page. The font size does not change.
-
- : specifies the number of traces to print per page. Some of the available selections are 1, 2, 3, 4, 6, 8, 9, and 16 traces per page.
- : sets the separation between traces when is greater than one.
Headers
-
: sets the text for the left, center, and right page headers. Type your own header text or select one of the header variables. Multiple header variables can also be combined with your own text.
The available header variables are as follows:
- ${AppName} - the current text in the 89600 VSA main window title bar
- ${Date} - the current date
- ${Time} - the current time
- ${DateTime} - the current date and time
- : When is cleared, the trace title will not be shown in the trace printout. This parameter is applicable only when is set to .
Preview
A preview of the printout is available when the collapsible section is opened. The print preview window contains functionality that searches for text within the printout, copy selected text, zoom in and out, and change the way page are laid out in the preview window.
Clicking the button opens a separate, resizable dialog that contains a print preview window.
Other controls
- button: prints the traces with the current settings
- : when selected, the printed trace includes the trace tab. When cleared, only the trace contents are printed.
-
: When this is selected, the background will be white. Very light colors will print black so they can be seen.
When is cleared, the trace area is printed using colors exactly as they appear on the screen.
Large areas of black do not print well on inkjet-style printers. If your printer is an inkjet-type, your print quality will be better if is selected.