Recall Constellation File

Recall Constellation File imports constellation files (*.txt) created using Keysight Signal Studio software. This feature is especially useful for very high order (VHO) QAM signals where large constellations are slow to load from a .setx file.

This menu item is only available with certain measurement types (e.g., Custom IQ).

The 89600 VSA supports constellation files saved using the following Signal Studio software products:

Signal 

Keysight Signal Studio Product 

Custom IQ

N7608B Signal Studio for Custom Modulation

See Also

About Save and Recall (Save and Recall)