Save Measurement
Saves the specified measurement into a VSA Setup file (.SETX). The settings saved in the setup file are the same as clicking if the specified measurement were the only measurement defined, with the following notes:
- The traces for the specified measurement are saved but the layout of these traces is not included in the setup file.
- Traces that use the specified measurement's results indirectly (i.e. math functions) are not included in the setup file.
The Save Measurement function, along with the Recall Setup (and option), can be used to combine measurements into a single setup file or to separate measurements into multiple setup files.
See Also