About Export

The Export menu provides options for exporting pulse tables and Pulse Descriptor Word (PDW) files when the Pulse measurement type is used and a pulse table is selected.

The Export menu is only visible when the Pulse measurement type is selected. Export choices are grayed out until a pulse table is displayed (Trace > Data > Result Tables > Pulse Table) and selected.

From the main menu, click File > Export to export the following:

Export

Pulse Table...

Pulse Descriptor Word File...

Pulse Descriptor Word File (Entire Recording)...

See Also

About Menus (Menus)