About Capture (Acquisition)
The Capture tab lets you enable and configure time-domain parameters for segmented time-captures. See Segmented Data Acquisition for more information about fixed length and variable length segmented capture.
Segmented Capture setup parameters are located in the Capture Tab.
In Vector mode, the segment shown in the Main Time and Spectrum traces is determined by . To see all segments in a single trace, select
See Also